AXIS#.IL.COMPTABLE.MAX

Description

AXIS#.IL.COMPTABLE.MAX sets the cogging compensation/torque compensation table index maximum. The table ends at the defined maximum axis position.

When AXIS#.PL.FB is equal to AXIS#.IL.COMPTABLE.MAX, the output of the table will be equal to the last table entry.

Example

To set the of the table to 360 degrees, the user would enter:

-->AXIS1.IL.COMPTABLE.MAX 360

Versions

Action Version Notes
Implemented 02-07-03-000

General Information

Type

Read/Write

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

Linear: counts, mm, µm, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value

360.0 Degrees

Data Type

Float
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
AXIS1.IL.COMPTABLE.MAX

500ah

1ah

Signed32

Position

-

Read/Write

No

AXIS2.IL.COMPTABLE.MAX

510ah

1ah

Signed32

Position

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.IL.COMPTABLE.MAX

5839

16CF

Signed32

Read/Write

Position

AXIS2.IL.COMPTABLE.MAX

71375

116C

Signed32

Read/Write

Position

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.COMPTABLE.MAX

5839

Signed32

Read/Write

Position